cancel
Showing results for 
Search instead for 
Did you mean: 

2 UARTS

kobi_hayun
Associate II
Posted on May 28, 2006 at 22:16

2 UARTS

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
kobi_hayun
Associate II
Posted on May 17, 2011 at 12:09

Hi All,

I am working with uPSD3400 and I intend to work with the two UARTs.

Is it possible to use one timer (TIMER2) for both of the UARTs?

They are working with the same baud rate and not working at the same time.

Thanks

KH

hanwayh
Associate II
Posted on May 17, 2011 at 12:09

Yes, if you set them to operate in mode 1, which is the standard asynchronous mode.

Han-Way Huang