Posted on March 29, 2005 at 13:38Hello, I finally managed to compile and run the USB-Bulk-Demo mentioned above. Enumeration and loading the driver was succesfull as well. I still do not understand how the PC-programm (RwBulk.exe)works. It says: Usag...
Posted on March 23, 2005 at 11:14Hello Hich, Quote:On 23-03-2005 at 14:43, Hich wrote: Hello Hkoch, You are right the demo was developed using RVDK, For the moment we didn't use onother tools. Could you let me now if you can load any program in the...
Posted on March 23, 2005 at 09:51Quote:On 23-03-2005 at 11:42, Hich wrote: Hi HKoch, - how do i modify the USB-Bulk-Demo to run from FLASH? you have just to change you scatter file address. I think this works on RVDK, but i can't get it running wi...
Posted on March 23, 2005 at 06:33Quote:On 23-03-2005 at 10:42, Hich wrote: Hello HKoch, You speak about The USB-Bulk-Transfer-Demo but I can't find a related document or code in the web, please can you say me where I can find this Cheers, Hich. ...
Posted on March 23, 2005 at 05:15Hello! I plan to use USB-Bulk transfer to transmit data from STR711 to PC. Using the USB-Software-Library seems to be difficult because ther are no raw template-files but only one application example using Interrupt-...