Posted on March 01, 2005 at 05:51Hi, If I save directly option byte by 'save as...' option (file menu) with ST7VP software, it work. The FMP bit has the good state :Read-out protection disable. I can reprogram the firmware any time i want! Thanks. R...
Posted on March 01, 2005 at 05:04Hi, ST7VP software doesn't save FMP state in option byte file, when I load project from this software, FMP state is always to read-out protection enable. I have to change this state to program option byte. Regards
Posted on February 25, 2005 at 10:35Hi, I've got a problem,I would like to download my firmware using SDK ST7VP_Toolkit without FMP Read-out protection, But each time I download firmware (with option byte) the device is write protected. With ST7 Vis...