Posted on February 17, 2005 at 10:25Thanks. I have mailed Metrowerks regarding this issue. I also asked them if they got an old Hiware compiler version from around 2000 they could send me. The code is compiled using Hiware compiler (year 2000). Sinc...
Posted on February 13, 2005 at 10:22Hi. Im trying to compile the soucecode for the 5in1 evaluationboard. The code is written for the Hiware compiler so im using Metroverks STM V2.0 and the compiler that comes with it. hw_st7_compiler v.5.0.12.4242. ...
Posted on February 09, 2005 at 09:09Hi. Im develomping an MP3 player using the source code from ST´s NAND flash memory example. I was actualy rather amased over how much code was needed for a memory stick. My problem is that I need to add a functio...