Posted on January 24, 2005 at 09:28hi Hich, thanks for your replay, just a precision, did i need to imlement an TCP/IP stack to use the HDLC for Point to point or multipoint conection ? or it is used with a special library with standard API ? thanks...
Posted on January 19, 2005 at 12:45i'm tring to understand what is the use of the HDLC peripheral.. is it possible to use this peripheral to connect on an Ethernet LAN ? did the processor include all the hardware for that ? that means we can connect...