Posted on October 03, 2005 at 14:30Is there a way to disable the double-register compare mode, other than by making sure the modes do not match on the registser pairs? Example: I'm using CC16 as Compare Mode 1 and want CC24 as Compare Mode 0, but do...
Posted on January 13, 2005 at 14:38The problem is resolved! This issue was that two channel injections were being run in two separate interrupts. The first channel injection event was being written over as the second channel inject event occurred si...
Posted on December 18, 2004 at 15:06 ST10F276 resets while doing an A/D Channel Injection Read. The micro is running at 64MHz and I'm doing a conversion via channel injection mode while the normal conversions are setup to Auto Scan Single Conversi...