Posted on May 17, 2011 at 09:50Is that also true for the STR9 family? If so, no way to use ST-like ISRs with the Keil's RTOS working? So the ISRs should be set up with the Keil's format... Thanks
Posted on May 17, 2011 at 09:50Hi, Has any of you resolve the problem with the interrupt enable? I'm having the same problem as you both. No way to enable the interrupts. First, with the example from the ST library UART (interrupt mode) only one int...