Posted on April 26, 2005 at 09:35Quote: You can view the current stimuli of you debug session using the command ''gdi pin -stimuli'' for all stimuli, or specify the pin you want to review and save in a specific file the result displayed in the conso...
Posted on April 21, 2005 at 06:13When using the simulator on ST7 visual develop 3.1.1, is it possible to save the I/O stimulation configuration? I notice that there is a menu item for ''Load Stimuli File'' in the file menu, but there does not seem t...
Posted on January 19, 2005 at 06:03We are having problems installing STVD7 on a machine running Windows XP pro. When the installation gets to the stage that it wants to istall the parallel port driver, the system crashes and reboots. The driver does...