After unprovisioning, we have to initialize several part especially the GATT Database to advertise the correct MESH UUID service and characteristics. NVIC_SystemReset() is an "easy" way to be sure that the Node will start with the correct configurati...
Hi,As per the error: L6050U: The code size of this image (174134 bytes) exceeds the maximum allowed for this version of the linker.It seems, IAR & KEIL are able to compile the code only up to 64K due to license unavailability.For IAR: Time limiting o...