Posted on November 08, 2004 at 09:19Dear WoRo, the advice was helpfull, but now I encountered another problem: the board is working with the inDart connected but when I leave the Metrowerks enviroment and Power up, the MCU stop working. the option b...
Posted on November 08, 2004 at 05:04 Hello All, I encountered a difficulty to use the MCO function. I set the option bytes to RC oscilator, PLL ON, PLLX8 and set the MCO bit in the MCCSR (MCCSR |= 0x02 , BUT no clock is out!!! Please Advis...