Posted on May 17, 2011 at 10:17Hi, i checked the current in sensormode: With the parameters in the attached file, the motor is running. But if i set the delay coefficients to 1 the GUI crahses. The shape of the current isn't what i expected. but i a...
Posted on May 17, 2011 at 10:17Hello, the motor i am using is a 70 V motor, the power of the motor is about 200W. I'm doing some more tests in sensormode to evaluate the current for successfull starting. Offsetvoltage: the Offsetvoltage seems to be ...
Posted on May 17, 2011 at 10:17Hello, thanks for your tip, but it is still not working. I set kp to 20 but the PC-SW is still crashing. Then i tried to run the motor in sensorlessmode, see item 2. Sometimes it still crashes, but not that often. I se...
Posted on May 17, 2011 at 10:17Hello, i'm running the ST7FMC Starter Kit by Softec Microsystems and have some troubles with GUI-crashes. These crashes seem to be depending on the Parametervalues choosen. I have two motors which i want to drive. Firs...