Posted on May 17, 2011 at 11:36We have experienced a failure with an ST9 F150. Code was running at one time, but with a few power cycles, the part is failing to start. An EPB can not communicate with it and no sinal is generated from the micro when ...
Posted on May 17, 2011 at 11:36Message: I\'m using the ST9 EPB with a 64K F150. When selecting the ST92F124/ST92F150 64KISP, it does not show flash memory from 0xC000 to 0xFFFF. Why?