STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
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
lionel
Associate
since
2018-07-19
2023-06-14
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About lionel
Options
Report User
User Activity
Posts
Replies
speed limit for BDLC control ?
2004-10-29
Posted on October 29, 2004 at 12:47speed limit for BDLC control ?
Re: speed limit for BDLC control ?
2011-05-17
Posted on May 17, 2011 at 10:17 Hello, I would like to use the ST7MC for BDLC up to 13500 rpm (this is a low torque and low voltage BDLC motor with 12 poles); Was is the limitation on the ST7MC to control the speed at this rpm (graphic s...