Posted on May 17, 2011 at 10:19You will find here attached the firmware source in assembly language of Starter_Kit tool. You will find inside all routine to communicate with the PC screen Graphical User Interface (GUI). The source code for PC GUI is...
Posted on May 17, 2011 at 10:19Hello, In closed loop the PI loop make a test with a minimum duty cycle. It could be that the minimum value set in your program do not allow to run the motor at lower speed than 800/1000rpm. You have to change this val...
Posted on May 17, 2011 at 10:18Quote:On 03-08-2005 at 11:30, Anonymous wrote: Could anybody suggest me links, infos about 12-step motor control mode. You will find in the attached patent (US 6,570,353 B2 from May 27, 2003) a 12-step drive.
Posted on May 17, 2011 at 10:18I send to you the zip file with source and project workspace allowing to assemble soft for ST72141 running on the Kanda kit Hardware. You have to know that this software is running using the SPI communication. Data of ...
Posted on May 17, 2011 at 10:17 Hello, The ST72141 microcontroller is dedicated to Permanent Magnet BLDC motor sensor or sensorless drive. The ST7MC allow to do the same drive with additional features like more BEMF sampling method, digital...