Posted on May 17, 2011 at 12:02When installing PSDExpress, the PC i unable to log in to Windows. I have tried both PSDExpress verison 8.10 and 8.02. When i enter my password on the log on dialog in windows, the PC hangs. The only solution is to rese...
Posted on August 09, 2005 at 10:40 OSC 1 is connected to the ICC connector. And i have tried to connect OSC2 to ground. Stil same problem. The ICC connector is connected as show in the application note (ST7 FLASH STICK User Manual), see attached...
Posted on August 02, 2005 at 12:55When trying to program ST72F264G2 using ST7 STICK, following error occurs: Error : Cannot communicate with the device ! Option Bytes are Disabled on the device Check the ICC cable connection and check all the needed...