Posted on October 27, 2005 at 17:41Having problem implementing a scat file to load code both in STR710 internal flash and external flash. A single area either internal or external works but together does not. Using RVDK 1.7. The Error message is: ''...
Posted on October 26, 2005 at 18:51Having the same problem as jeetendra posted on 06/04/05, but with RVDK 1.7 Trying to load program in the external flash on the STR710 evalution board. Using RVDK 1.7 for development and internal flash work OK. Are ...
Posted on March 29, 2005 at 13:36Having problems writing message to the MB393 LCD display and processing interrupts concurrently with LCD I/O instructions. The processor resets. Any known problems with this type of thing? :-(