Posted on February 13, 2008 at 13:17I was but I had to remove it as it kept reseting due to noise on the power line! It was a Max1232 which ''browns out'' at 4.75v and I think noise spikes were setting it off I am changing it to a different device w...
Posted on February 07, 2008 at 11:27We are having problems with STR730 devices wiping part of their Flash memory when they power-up, usually including the lowest addresses which means they wipe their Reset Vector!! Does anyone know what can cause th...
Posted on August 20, 2007 at 15:09Hi, thanks for that, I failed to find the thread when I searched for anything related. It is exactly the problem I seem to be having and exactly the solution (8 nops = 2 instruction pipeline * 4xcpu clock). It seems...
Posted on August 20, 2007 at 08:38you don't mention whic processor you are using... We had problems with the STR730 because there is a mistake in the C library where the TOR address is not specfied correctly. Make sure you have the latest library up...
Posted on August 20, 2007 at 07:58We are using an ARM712FR2T6 in a design and due to lack of thought in the hardware design we now find we need to modify pins of an output port during both normal and IRQ processing. I have masked the port modificati...