Posted on August 25, 2004 at 15:08Hi, The EEPROM M24C08 needs to receive the device select Code in order to receive This Device select codes corresponds to the Address (which is sent directly after START generating) page 242 STR710F hardware referen...
Posted on June 30, 2004 at 13:30Hello shinn, I think also that what you have done in the project proprieties can be done using the scatter file (scat.scf) as following for example . Flash 0x40000000 0x10000 { Flash 0x40000000 { 71x_vect.o (Vect, ...
Posted on May 06, 2004 at 13:39Hi For the TIMER case, As it is said by ''RISC'' some function of the library are coded in the header file when the are inline . I see that the function such as TIM_ICAPValue and the other clock configuration function ...