Posted on May 19, 2004 at 07:37In the inDART-STX I have the possibility to choose ICC Mode Entry. If I choose ''Ignore Option Bytes'' which configuration is then taken? For the project I would like to have the possibility to use the external Clock o...
Posted on May 18, 2004 at 13:22Can anybody tell me for what this special sector is (it has to be setup in the Option Byte). If there is somewhere a decription pls specify where I can find it. Kurt
Posted on April 13, 2004 at 12:37I can't believe that. If I have to ADD/SUB 2 packed-BCD Bytes there must be a possibility together with the CC register to adjust the result to a packed BCD-Byte. On 2004-04-12 13:18, Jatin wrote: There is no dedicat...
Posted on April 08, 2004 at 16:46the ASM language of the MC05 and Z86 I have programed until now there is instruction for decimal adjust after SUB and ADD operations. How can I do this at the ST7 ?