Posted on January 12, 2004 at 12:32Thank you all I'm using the ST72F521R9T. I used the large model (''+modml''). it has been linked,but it doesn't work in run time. I tested same software which is compiled in all models. Only ''+modml'' is cruched i...
Posted on January 11, 2004 at 07:10 I'm trying convert package software which has compiled by metrowerks to the cosmic compiler but I get these errors: #error clnk C:\PSD_Data\Cosmic\kpad\Config\kpad.lkf:1 segment iram size overflow (451) #e...
Posted on December 20, 2003 at 18:40 you can look the prm file in the attachments. I compile my project (-ml) LARGE model. atz
________________
Attachments : kp.prm : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00D...
Posted on December 19, 2003 at 10:35 I use ST72F521 that his stack allocation is in 100-1FF. When I try to define in project.prm SECTION as follow: SECTIONS MY_ZRAM = NO_INIT 0x80 TO 0xFF ; MY_RAM = READ_WRITE 0x200 TO 0x87F; MY_ST...