Posted on May 17, 2011 at 12:01EEPROM cont. Hi Moderator, thanks for you pointers. Here is what I have in mind. I intend to grap data 32 bytes each time. I will enable SPI interrupt and serve this interrupt. doing this I can grap data in the backgro...
Posted on May 17, 2011 at 12:01Hi Guys, I am doing an interface between MCU and an EEPROM, using SPI. In the application, there must be RTC, timer interrupt, and SCI interrupt. My data is gonna be in the EEPROM and I have to search for it every 5 se...
Posted on May 17, 2011 at 12:00 Thank You Maybe I will ask you some more question when I do this. Since you have done it. If you don't mind. Thanks again.
Posted on May 17, 2011 at 12:00 Hi I am using the uPSD3212, and planning to have the primary flash as program space and the secondary as the data space. The primary flash is devided in to 4 sector of 16K and I am planning to stack them up from...