Posted on May 17, 2011 at 12:03I think you're right, the problem is almost certainly that very large capacitor. The reset will work without a reset supervisory circuit, so unless there's a good reason to use it, there's no need for it.
Posted on May 17, 2011 at 12:02The original ST example code had some problems with the USB interface due to too much time being spent in the USB interrupt service routine. They did a radical re-write and have re-relased the example code. I assume if...
Posted on May 17, 2011 at 12:02In uPSD32XX the alternate functions can be set up either by writing to registers at runtime, or by PSDsoft express. Some can only be set by writing to registers.