Posted on May 17, 2011 at 11:35 thaks Sergio for your interesting. I read the document and is vary usefull. But the chip that I have are all with Y letter, and i beleave that the problems is not the same. You have other idea!? Tanks !! ...
Posted on May 17, 2011 at 11:35 I hve a problems whit ST9f120V1,after a few day that he work normaly ,he lose a parte of code. I have product 100 control board and 15 of this have this problem Is possible that MCU lose the code burning in flas...
Posted on May 17, 2011 at 11:34 I use the ST92F150 and i have a problems with the rx interrupt on SCI- A . The tx interrupt run OK .I set the RE RIE TCIE TE bits on SCICR2 and I set the Interrupt bit on SITRH=0x01 SIPLRH=0x02 SIMRH=0x Can you help...