Posted on January 13, 2005 at 05:51 Dear bugaloo, I tried this program yesterday. Thanks for the hint! There are many ''assertion failed'', because it checks, if the parameters are useful. But this prevents entering the parameters, if you h...
Posted on January 11, 2005 at 19:49Do you have a VGA register set example for a 1024x768 display ? Perhaps in a 32kBios, even with 63 Hz. Best Regards Flipflop
Posted on December 18, 2003 at 08:57Hi. The STPC has an VGA-Controller and the output is then feeded into an LCD scaler. In most times, the CRT has more pixel than the LCD. The idea is: Set up an analog VGA Picture on you CRT with the desired resolu...
Posted on November 26, 2003 at 04:16Hi! It depends on the operating system. The TFT parameters are included in the last part (32kB?) of the BIOS-Chip on the Evaluation Boards. Split a ROM image into BIOS and the VGA-Bios. There is a Windows utility ...
Posted on November 24, 2003 at 06:56Having an own type of LCD, not supported by ST, it is required to compile the stuff on our own. But - the directory structure changed between Xfree86 4.0 and 4.3. It won't compile. I sent my LCD data to a ST repre...