Posted on May 17, 2011 at 11:57 Hi everybody How can I do an internal reset after an extenal interrupt ? (The external interrupt must accomplish same opperations before the reset) Thank you all Kobi
Posted on May 17, 2011 at 11:56 Hi I am trying to use two PWM ports at the same time. I initialized the PWM 0 and 1 and gave than the same duty cycle (255) In one port I received 5v and in the other 0v.I need that both outputs will be 0v....
Posted on May 17, 2011 at 11:56 Thank you all According to an1560, the xdata is also for the main flash memory and I wont to access the 8Kb SRAM with the battery backup. Thanks kobi