Posted on August 03, 2005 at 06:25One can not debug SPI code on the ST72F231 because the debug program uses the SPI ports for communications. Maybe, you are having same problem with your device. Good luck, DaveF
Posted on July 24, 2005 at 08:37WoRo, Thank you for the detailed explanation. I think I finally understand what is happening now *** I think you can solve your problem very easily if you know how the whole PWM generation depends on the ART COUNTER...
Posted on July 22, 2005 at 08:19WoRo, First off, I agree with and/or understand all of your latest comments. My main problem is why do I have to put more than 5 into the PWMDCRx register (in my example) to start getting pulses out of the PWM? page 6...
Posted on July 21, 2005 at 09:48WoRo, On page 66 of the manual. DUTY CYCLE REGISTERS (PWMDCRx) Read/Write Reset Value: 0000 0000 (00h) However, I find that I need to add 5 to the duty cycle value that I put into the PWMDCRx register if I want to get...
Posted on July 18, 2005 at 09:17WoRo, *** To read the port value I only change the output from DDR/OR: 1/0 (open drain output) to 0/0 (floting input) and backwards keeping DR=1. *** That is a safe transition for you, so all you need to do is change ...