Posted on July 17, 2003 at 08:58Hi, Since I seem to get answers quicker on this forum, I wish ask one more question about Port0. Port0 acts as 16-bit data bus in demultiplexed bus mode. But it can only work as 2 8-bit ports when used as ports. This ...
Posted on July 17, 2003 at 08:40Hi Kenshin, Thanks for the reply. You are right about the trap number. I had assigned it as 0x28 instead of 0x1C. 28 is the decimal equivalent of hex 1C, hence the confusion. I was not able to detect this error earlie...
Posted on July 15, 2003 at 10:17Hi, I'm using Timer T6 to generate a clock for a device and I want to keep a count of these clock pulses. Also I want to use CC12 as positive edge interupt (P2.12). I have kept the priority of this interupt higher tha...