Posted on May 17, 2011 at 12:01Sorry! the previous message has been posted by mistake. I actually got a problem with reading Main Flash. At 0xFFFB I store a number to indicate a valid firmware copy, and boot program read from there during power-up. ...
Posted on May 17, 2011 at 12:01My application program originally run from the Boot Flash(csboot0-3: 0x0000-0x7FFF). To implement IAP I download it into Main Flash using the bootloader which resides in Boot Flash. Then the bootloader pass the control...
Posted on May 17, 2011 at 12:01I've stuck on IAP for few weeks. I even sent the relevant code to ST support, but nothing helpful back from them. Does anyone here implemented IAP completely on uPSD2324A ever? My application programme can run from sec...