Posted on May 17, 2011 at 12:31hi all, I'm trying to test the CAN bus on my hardware. I use the CAN example program available in the FWLIb. My hardware is based on the STM32F103VBT6 and the CAN is mapped on PD0 and PD1. Here is the GPIO initializati...
Posted on May 17, 2011 at 12:30Thanks for the information. I still have a problem with the microSD size detection. Indeed window XP detects a 4Gb MicroSD even though i use a 2Gb microSD. any ideas ? greg
Posted on May 17, 2011 at 12:30hi all, I use a code similar to the one provided by USB Mass storage Demo. I use on my board a 2Gb microSD card. I noticed that when i connect my board for the first time on the USB port, XP indicates that there's a pr...