Posted on May 26, 2003 at 05:05Hi, thanks for your reply. The Vpp voltage is generated by the circuit board on which the ST7 is attached. The entry pulses are performed by a digital test system which can stimulate all necessary pins of teh ST7. So i...
Posted on May 23, 2003 at 12:24 I want to download the complete program code into the HDFlash of an ST72F324 with ICC-Protocol but no PC or programmingboard. All necessary pins of the ST7 are connected. My idea is to connect ICCDATA and ICCCLK to ...