Posted on November 10, 2003 at 07:18The uninstall message does only come if you start it the second time!! So if you start it the first time there should be printed: STPC DMA Verify - INT13 installed I compared the reg values. The FDC-Reg F0 is set ...
Posted on November 04, 2003 at 05:43 I remember 2 problems: 1.) Floppy-DMA-Verify doesn't work because the Elite-DMA did'nt support this mode. I wrote a little DOS-TSR-Programm STPCDMA.EXE which prevents the use of DMA-mode. The problem is also ...
Posted on September 12, 2003 at 08:11 I had same problems with STPC Industrial and STPC Elite with Winbond W839 Please check attached keyboard driver for dos.
________________
Attachments : kbd16.zip : https://st--c.eu10.content.force.com...