cancel
Showing results for 
Search instead for 
Did you mean: 

STPC Elite - DDC lines

moedeker2
Associate II
Posted on June 03, 2003 at 10:24

STPC Elite - DDC lines

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
moedeker2
Associate II
Posted on June 03, 2003 at 09:01

Has anyone experience with the DDC lines of the STPC Elite. I could'nt access them. They are always high (due to the pullups). The will never toggle to low. I used chip register 95h.

Bernd

stephen239955_st
Associate II
Posted on June 03, 2003 at 09:54

There is a mistake in the documentation. They are controlled via register 97h not 95h.

moedeker2
Associate II
Posted on June 03, 2003 at 10:24

And the bit sequence is inverted.

Bit 0: W_DDC1(CLK)

Bit 1: W_DDC0(DAT)

Bit 2: R_DDC1(CLK)

Bit 3: R_DDC0(DAT)

Why could this not be found in the Elite errata?