Posted on May 22, 2003 at 13:17Hi all. I am programing a ST7 and i get this problem using the ST7 Assembly Chain: Error 54: Can't match Addressing mode ' LD A,([ptr.w],X)' ptr has an address of memory (E100h) and is located in the address 01D2h X=i...
Posted on May 06, 2003 at 05:40 I think is a problem with the micro i am using, the ST7262 Because i also get this error when entering in the debug mode ''failed to download application: error: gdb7 internal error: not a supported microcontro...