Posted on April 12, 2007 at 11:18There is no flash device in the ST6 serie. I recommend you start new designs with the ST7. It seems that there is no new development in the ST6 serie. We have just converted all our ST6 designs to ST7, which means se...
Posted on February 16, 2007 at 11:16There is no way in the ST7F325 to select one pin in a group sharing the same interrupt as in ST7FLITE. You select which pin will generate an interrupt with the option register. If option register bit is 0, pin con...
Posted on July 08, 2006 at 10:35Hello Look at application note AN2288 Single-phase energy meter with tamper detection based on ST7FLITE2x. You will find lot of good insights in building an AC energy meter. Clever circuit will enable good resolution ...
Posted on December 26, 2005 at 16:31When using STVD7 and SIM to debug my programs, I cannot get the display of the peripherals registers in the peripherals register window using the ST7FLIT19BF1 MCU. It says : ST7FLIT19B1....No port defined. If I se...