Posted on May 17, 2011 at 10:17For your drivers, you only need to update MPOL register value in the original library (line 382, mtc.c). You need to update the watchdog value accordingly. (MCO output state after reset)
Posted on May 17, 2011 at 10:17First of all, make sure you don't have a hardware problem -> do not change anything from the original library and program the ST7MC1 with your motor settings (for the moment all the chips come with the same die (will c...
Posted on May 17, 2011 at 10:14Hello, The fact is that the undervoltage fault is ON under 20-21V, to make sure that the alignment of the included PMSM motor is done properly (enough current). So if you want to run another motor, you may have to remo...
Posted on April 24, 2003 at 10:50 Please can U check first this attachment? (map files for different mcus, including st7flite2) Rgds F
________________
Attachments : mapfiles.zip : https://st--c.eu10.content.force.com/sfc/dist/version/do...