Posted on October 07, 2003 at 15:16Hello, To reduce thermal dissipation and power consumption of the STPC Elite, I would like to follows the datasheets advice, and to shutdown unused interfaces and functions. The datasheet recommends to ground some ...
Posted on June 25, 2003 at 11:08When accessing the PCI configuration registers - register 0xCF8 has 6 bits for the register number (bites 2...7). It means that the highest register number that can be accessed is 0x3F. How can I access the SOUTH BRID...
Posted on June 24, 2003 at 08:18To access register 40h, what values should I set to Register 0xCf8 - Enable - 1??? Bus number - ??? Device number - ??? Function number - ??? Register number - 40h Thanks!
Posted on June 24, 2003 at 05:50Hello, I am using the STPC Elite. I would like to configure the registers controlling the GPIO. However, the values that I set in the control registers are never set, and the default value always stays there. For exam...
Posted on April 28, 2003 at 04:01In STPC Elite - when setting MEM_REG0, there are 3 possible configurations for the memory bank configuration (bits 18-17, Mnemonic - Config). The SDRAM that is use is 512K Words x 4 banks x 32bits. This configuration...