Posted on May 17, 2011 at 11:54If you use version 7.6 or earlier of PSD Seoftexpress you can reallocate the JTAG pins on the device. This functionality has been disabled in leter version of PSD softecpress as it seems to be very easy to 'lock' the u...
Posted on May 17, 2011 at 11:53Hi, The spec you need does obviously exist, but it is VERY complicated. The programming of the FLASH via JTAG is easy the problems come with the JTAG programming of the CPLD which is very complicated. Is there no way y...
Posted on August 18, 2003 at 06:40Hi, Your problem is the 12MHz clk on the Indart ST7F and the 16MHz clk on your application board are conflicting with each other. The solution to this problem is to construct a second cable for connecting the indart...
Posted on March 26, 2003 at 08:36This refers specifically to mixed ports, ie Input and Output on the same port. If the port is all output then you can use the Bit Set and Reset commands with no problems. If however you have mixed ports, the suggeste...