Posted on May 21, 2003 at 13:06Hey there, I am trying to connect the st10f269 to a DUART froom Philips. The Duart accepts 8 bits which will come from the 16-bit data bus of the st10. The question is which Bits should be connected to the DUART. There...
Posted on April 10, 2003 at 14:13Hello there, i was wondering if anyone has found any ST10 libraries for the protel PCB software(99 or dxp)? Thanks in advance Vasilios
Posted on March 31, 2003 at 11:50OK here is the code bit which confused me: / * this. Timeout is set to 5 msec assuming a 20 MHz bus /// --------------------------------------------------------------- /// Configuration of CC1 timer 0: /// -------...