cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 connected to DUART

el98650
Associate II
Posted on May 22, 2003 at 13:12

ST10 connected to DUART

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
el98650
Associate II
Posted on May 21, 2003 at 13:06

Hey there,

I am trying to connect the st10f269 to a DUART froom Philips. The Duart accepts 8 bits which will come from the 16-bit data bus of the st10. The question is which Bits should be connected to the DUART. There is the obvious Software Solution to shift all characters i write so that the data to transmit is in the lower 8 bits, but i was wondering if there is a better solution. Any Ideas or hints are very appreciated.

el98650
Associate II
Posted on May 22, 2003 at 13:12

Ok figured it out myself.. If someone is interested in the solution just mail me..