Posted on March 04, 2004 at 05:04After investigation our STPC VEGA support DiskOnChip. The incompatibility issue between M-System DOC and Rise CPU core can be resolved using the new firmware version 5.XX from M-system. So Millennium 8MB and upper an...
Posted on November 21, 2003 at 10:39you could ask your local ST contact or distributor, all documentations are not yet on the web but existing internaly
Posted on July 22, 2003 at 08:49To provide you some more Info, The ethernet Mac controller is based on Tulipe Standard with some minor modifications. ST will support and provided driver for LINUX, WIN CE.NET and WIN XPe. Target is to have available ...
Posted on July 22, 2003 at 08:43To complete the answer, Yes STPC VEGA are not supporting DOC but as an alternative more and more customers are using Compact flash through IDE BUS. It is an other solution to work with Files managed as an Hard disk wi...