Posted on May 17, 2011 at 10:16 Here is the C-code void swapElements(int a[], int maxPos, int last); void bubbleSortPhase(int a[], int last) { // Precondition: a is an array indexed from a[0] to a[last] // Move the largest ele...
Posted on May 17, 2011 at 10:16 With a correct design, bemf detection is as reliable as hall effect sensors commutation, I have designs running up to 70000 rpm's where the motor never stalled. sensorless is the way to go
Posted on May 17, 2011 at 10:16 That is a difficult task, having 2 teams working on the same µcontrol program and trying to protect source code... In my opinion, things have to be dealt on two ways: -A Contract describing what each party are g...
Posted on October 31, 2003 at 05:02 I have tried both and finally choosed the cosmic ! I like the Cosmic thing, highly optimized towards code efficiency even their maths libs are impressive but their editor (idea) is pure BS.