nils
Associate II
since
2018-07-19
2023-06-14
User statistics
6
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About nils
Options
Report User
User Activity
Posts
Replies
iic slave code
2003-04-23
Posted on April 23, 2003 at 13:03iic slave code
ST62 OR command
2003-02-12
Posted on February 12, 2003 at 14:13ST62 OR command
Re: iic slave code
2003-04-23
Posted on April 23, 2003 at 13:03 Ok, wrote a small program that does the job, since I'm a firm believer in open source here it is... 3 Byte transmision: device address, data address, data read/write runs @ 10kHz (8MHz resonator) and does n...
Re: iic slave code
2003-02-20
Posted on February 21, 2003 at 06:25Speed is not critical, I was hoping for 100kHz, but can define it to run much slower.
Re: iic slave code
2003-02-19
Posted on February 19, 2003 at 11:07Am looking for i²c slave driver software in assembler for a st6200 (the smaller the better)
Re: ST62 OR command
2003-02-12
Posted on February 12, 2003 at 12:35Hi, anybody know how to get an efficient OR command going for an st6200?