Posted on September 29, 2004 at 14:32 For generating an s19 file in an STVD7 3.0.1 version, you can do the following: 1.Go to Project 2. Then settings 3. In th Pop-Up window, go to Post-Build TAB 4. In the description write ''Running Po...
Posted on September 28, 2004 at 10:54The Product supports the Automotive Temperature Range. But you need to verify the characteristics of I/Os, PLL, RC oscilltor etc. as per your application with different temperature. These are given in the Electri...
Posted on September 28, 2004 at 10:38There seems to be a connection error, so you can verify the following: 1. If you are using STVD7 3.0, In the Debug Instument Tab, select the Port at which you have connected the emulator. If you are using old ver...
Posted on September 09, 2004 at 10:20I do not exactly understand your application, but based on the specifications you have described following could be suggested: 1. ST10 a 16 bit microcontroller with 40MHz frequency, but it does not have an inbuil...
Posted on September 06, 2004 at 12:02The FAT32 specification availaible on Microsoft site. Also you can refer to Logical Format specifiaction of Smart Media Card (A type of Flash Card). This would be availaible on www.ssfdc.or.jp