Posted on May 17, 2011 at 11:54Hi, I am using the uPSD3200 - Part PSD3233BV. I have configured timer 2 for auto-reload (T2CON=0x00), enabled the interrupt (ET2 and EA), loaded Tx2 and RCAP2x. - Then enabled the timer (TR2). I have used this sequence...
Posted on May 17, 2011 at 11:53 Was about to give up on this - Then noticed the details of the P3SFS register. Once I conditioned the port pins to be used for I2C I started to receive acknowledgements. Silly me
Posted on May 17, 2011 at 11:53Has anyone had any success with code to use the uPSD as an I2C SLAVE? Whatever I try (and I've now tried a lot), I cannot get the uPSD to generate an acknowledge on receipt of a valid control (aka address) byte - Causi...