Posted on May 17, 2011 at 11:33Find attached ''mb276b.pdf'' epb schematics. For ST90E158LV low voltage devices (3.3V) the power supply has been trimmed on EPB in August 1999. The modifications was: 1) change resistor R7 from 2.00K to 1.5K 2) change ...
Posted on May 17, 2011 at 11:32Jojo You are wrong. Testflash is in emulation chip. On emulation chip only one control bit allows to enable/disable all internal Flash memory (i.e sectors F0, F1, F2, F3 and testflash and FlashOTP). So, to be able to r...
Posted on May 17, 2011 at 11:32When you go from editor to debugger your program is automatically reload in emulation memory (if memory is mapped as system) or in ST9+ internal memory (if memory is mapped as internal). note 1: V6.1.7 handles far bett...
Posted on February 21, 2003 at 12:18Hi You must connect VDD to ICC connector pin 7. ST7MDT10-EPB needs this VDD as voltage reference. Then, as you have not connected ICC connector clock (pin 9), you must use ICP OPT Enable. If you want to use ICP OP...