Posted on December 09, 2002 at 09:07Hi I'm using Hiware C compiler and indart-st7. I want to have example program(C environment /st7lite09 ) under file -. map /.prm / default.env / .mak .c .h (interrupt define file / SFR define file) ref: don't chan...
Posted on December 04, 2002 at 06:54st7/ INTEL #INCLUDE ''ST72FLT0.INC'' INTEL ; intel format WORDS ; segment byte at 80-BF 'ram0' BYTES .TEMP DS.B 1 ; temp Register WORDS segment 'rom' ; rom area main CALL ram_clr ; ram clear CALL timer_i...
Posted on December 03, 2002 at 21:04Hi I have problems with the timer interrupt.(AT TIMER Overflow interrupt) I am using indart-st7flite0 for st7lite09B. I want to ouput as port ''A'' about Temp(var). and generate 10ms time interrupt. ref. After exe...