Posted on May 17, 2011 at 10:16Hello, Please find attached the associated code. Be careful that this code is written in assembler and works with the Kanda Kit (ST7MTC2). Best Regards
Posted on May 17, 2011 at 10:16Hello, Can you describe more precisely what happens at start-up with your 24V motor? When you said ''It appears to make it through alignment then stops and tries again'', do you mean that after alignment, it is doing a...
Posted on May 17, 2011 at 10:16Hello! The speed is not related to the PWM frequency but to the PWM duty cycle and to the step time (meaning the time between 2 commutations). Example for a BLDC motor: For a 2P Poles MOTOR at N (rpm) targeted speed: S...
Posted on May 17, 2011 at 10:16Hello, No changes are needed in the software between a star and delta connections. Only the delay coefficient (which determines the delay between the back-emf zero-crossing detection and the next commutation) needs to ...