Posted on May 17, 2011 at 11:34 Find enclosed the source code doing so with MFT1. OUTA 50% duty cycle, OUTB 75% Jojo [ This message was edited by: jojo on 03-06-2003 23:21 ]
Posted on May 17, 2011 at 11:34 The ST92F150 Current consumption between these 2 modes are not the same. For Stop mode, MAX current consumption is 40 uA. For Halt mode, TYP is 6uA and MAX is 20uA Jojo [ This message was edited by:...
Posted on May 17, 2011 at 11:34 I have used STVP9 for many years and I do not confirm your problem. Make sure that you open the right file and this one was recently recompiled. For instance, if you use the code shell from http://www.stmcu.c...
Posted on May 17, 2011 at 11:34 Your problem comes from a limitation of STVP9. There are 2 ways to overcome it. 1. you implement in your boot code a subroutine in charge of copying your routines (the ones for erasing and writting the Flash...