Posted on August 13, 2003 at 12:34Hello, just one question: do you run the samples on STPC Atlas or Consumer II or anything else? I have checked the source code and it needs some changes in the vid3buf.c file to work on Atlas (and only this one): re...
Posted on May 12, 2003 at 08:13Hello Yahel, as said by Farfalla, the STPC frame buffer driver is selected in the append line of the lilo.conf file. example: append=''video=stpc:xres:800,yres:600,depth:16,refresh:60,ypan'' This example is provided in...
Posted on April 04, 2003 at 07:04 Hello Tresh, you are right, the memory mapped registers and the frame buffer space at 128MB must be declared in a descriptor table located in the file in syslib.c. I attached a detailed documentation that c...
Posted on November 19, 2002 at 13:20 Stephen, you need to follow the following steps: - power off the board - close the jumper - power on the board - check that the postcode 0D is reached - power off the board - open the jumper It should be OK now !...
Posted on September 25, 2002 at 10:42 Hi, I would like to know more about the Flash Memory: 1). When (because of stress or alteration) the Flash Memory give a wrong value, how can we see this fault: Bit error, a bit 1 is read 0, a bit 0 is read 1, a...