Posted on May 17, 2011 at 11:33You have to add the run-time library to your ''LIBS ='' line in your make file. Please add: # List of libraries LIBS = C:\ST9PlusV6.1.7\lib\gcc-lib\st9-elf\2.7.2\mmedium\libgcc.a and it will fix your problem. Also, ple...
Posted on May 17, 2011 at 11:33The manufacturer of these connectors is SAMTEC. The SAMTEC reference of the connectors are: SFMC-112-01-S-D for the 2x12 female connector SFMC-110-01-S-D for the 2x10 female connector You can get all the information on...
Posted on May 17, 2011 at 11:33The access mode used on the Eval board is not correct in regards with the RAM specification : the /DS (connected to /G) should not be low during the write access. Therefore, a modification to the ST9GP-EVAL PCB MUST be...